This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: Source of logic high for OTG pin

Part Number: BQ25895


The recommended approach to enabling OTG is to pull the pin high and write the OTG register. I would like to know the source of the logic high on battery based systems. Will a 10k resistor to PMID suffice ? Are there additional considerations ? Datasheets note that this pin can handle upto 7v and PMID should at least output battery voltage - mosfet voltage drop. So tying OTG to that should achieve a logic high for 5v output on PMID purposes.