Other Parts Discussed in Thread: BQ24610
Hello,
I need to develop a sealed lead acid battery charger which will be incorporated to an UPS module of a medical device. The charger will charge two 12V/12Ah batteries connected in series. Each battery has 6 cells.
The maximum charging voltage is 28,5V and the charging current is 4,8A (maximum).
I was wondering if I can use the BQ24450 in this design. Is it possible?
If no, what TI component should I use?
Thanks in advance,
Luis