This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TPS56637 is a high efficiency, high-voltageinput, easy-to-use synchronous buck converter with integrated MOSFETs.
With the wide operating input voltage range of 4.5 V to 28 V, the TPS56637 is ideally suited for systems powered from 12-V, 19-V, 24-V power-bus rails. It supports up to 6-A continuous output current.
Yes, recommend to add AE with ESR or TVS diode when the system is powered by 24-V long power lines. :) :)