Hello,
I am designing a portable system with two 3.7V Li-poly rechargeable battery powered. The plan is simple that the batteries will be charged (BQ25886) through USB or 5V adapter, and there should be protection (S-8252) to the batteries for overcharging and overdischarging. I have attached the design. I have two questions: First, the n-mosfet (for power controls -at the right bottom in the figure-) S1 goes to the negative side of another cell which is eventually going to ground, and S2 goes also ground (designed the protection circuit with referencing S-8252 datasheet). So, how do these mosfets control charging and discharging? Second question, is there any missing connection on the design especially VDD at the protection to the SYS pin of the BQ25886? Could you share your feedback?
Thank you,