This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Team
I would like to ask about output capacitor of BQ25606.
Checking the following application of BQ25606, a 10 μF capacitor is connected to the output capacitor on the SYS side.
However, the following description in the data sheet mentions 20 μF or more.
Which should I design based on when actually designing?
What is the problem when using a capacitor of 20μF or less?
Best Regards,
Y.Ottey
Y.Ottey,
It should be <=20uF.
Please visit https://e2e.ti.com/support/power-management/f/196/t/890626 for BQ25606: Schematic Review and PCB Layout Design Tips. Additional Information including FAQs is available http://www.ti.com/lit/an/slva924/slva924.pdf Designing A Standalone Single Cell 3-A Charger with the bq25606.
Thanks,
Ning.