This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92074: My customer is looking for a LED driver like TPS92074.

Part Number: TPS92074
Other Parts Discussed in Thread: LM3445, LM3414

 Hello guys,

 One of my customers is looking for a LED driver device which has the following features.

 1. It is the device which has the buck topology with a external NMOSFET like TPS92074.

 2. Vin = about 200V DC.

 3. Vout = total LED Vf = 40V ~ 120V

 4. The device must have PWM diming function.

 5. It is beter that he device has analog (Linear) diming function.

 Do you have any device like the above?

 Your reply would be much appreciated.

 Best regards,

 Kazuya.