This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5066I: Start up problem

Part Number: LM5066I
Other Parts Discussed in Thread: CSD19536KTT, LM747

Hi, I've been debugging a startup problem with the LM5066i. The gate pin seems to have a hard time starting up and so far I couldn't figure out the cause. PSPICE stimulation shows the expected result but unfortunately that is not the case with the physical circuit. As long as VIN is between the UVLO and OVLO, VOUT seems to be stuck at 4.1V and Gate at 7.2V


My MOSFET of choice is a CSD19536KTT. Below is the scope screenshot and the design summary. Any leads would be appreciated. Thank you in advance.