This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We designed a 24V to 10V regulation circuit using TL431BIDBVR as suggested in Figure 27, Page 25 of the datasheet. Our design is also enclosed for your reference. Below are the major required parameters :
VIN = +24V
VOUT = +10V
Iout = 25mA
We would like to understand this design will work?
Whether we can generate 25mA to 30mA of Load current using this design. Please confirm.
Regards,
Hi Vijetha,
The design will work. Just keep in mind that you will be putting close to 0.5W onto R403.