This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: TL431 applications that output more than 60V

Part Number: TL431

Hi 

It seems that the highest withstand voltage of the TI 431 family is only 36V.
As the output voltage needs to exceed 60V, must be added to the voltage regulator at the feedback circuit of TL431.
I would like to ask if there is a higher withstand voltage 431 (or related application materials can also be used) to avoid additional voltage regulator circuits. Thanks.

Regards,

Rock

  • Hi Rock,

    It is rare to see a TL431 require more than 60V.

    Can you tell me more about the application?

    Is this a single rail output?

    Is there a sub <36V output voltage rail available?