This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24780S: can not charge

Part Number: BQ24780S

Hi Sir,

When the system power load increases, the Charger IC cannot be charged
The conditions are as follows
Adapter: 19V, 7.89A

when Rac seting 0.01Ohm and on Rac voltage as below:
1. At 40% system loading, 37.8mV, the battery can be charged 0.5A
2. At 60% system loading, 45mV, the battery can be charged 0.5A
3. At 100% system loading, 58.1mV, the battery cannot be charged

there any errors in the setting of the attached theschematic? Is the schematic correct? please kindly let us learn from you and suggestion to us.

MG4U_DVT_DC BOARD_0518-1430.pdf