Dear Specialists,
My customer is using TLV70033 and has a question.
I would be grateful if you could advise.
---
When the 3.3V output voltage and output current were examined on the board on which TI's TLV70033DCKT was mounted, it was found that the peak current exceeded the limit value for a moment.
Could you please see the waveform data measured in our company.
Is the TLV70033DCKT damaged at such an output current?
Although it exceeds the current limit, the time is very short (tens of μs at start up), so it is considered that there is no problem from the viewpoint of heat.
This circuit has been used in our products and is operating normally.
TLV70033 peak current operation.pdf
ーーー
I appreciate your great help in advance.
Best regards,
Shinichi