This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400: TPS65400 PSpice Transient Model simulation limitations

Part Number: TPS65400

Hello,

have problems to simulate 

SLVMAI5.ZIP (73 KB) - PSpice Model
with lower 9 Volt input voltage.
this windows appears only with input voltage on V11 (SLVMAI5) less than 9 volt.
My goal is to find good parameter:
  • very high efficiency at ~900kHz - 1000kHz
  • ~100kHz bode bandwidth
  • Cff for Ch.#0...3
  • COMP Network
  • inductor value

with

  • Input voltage 5.2...5.4 V
  • low ripple output voltage ~10mV 

for outputs:

1.25 V @ max. 3.6 A 
0.95 V @ max. 3.8 A
1.85 V @ max. 1.5 A
3.35 V @ max. 1.5 A
Thanks.