This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: ucc28780- ROOT CAUSE FOUND

Part Number: UCC28780

Ulrich:

ugh! We located the root cause of the situation where nodes were getting "stuck".

It is in the pcb routing of VDD connection to the Aux winding through the rectifying diode D1  & R5 and proximity of AUX trace.

.I suspect that the  via for the AUX output  that is  .25mm away from VDD trace in inner layers.

And that must be too adverse a  shunt impedance to the VDD line.  AUX coil other end is GND so it effectively shunts out charges ..do not see a short though.

If we disconnect that trace, we get back signature SWS and HVG waveforms....but is it the complete explanation?...need to explore more.

I will report more on this. An interesting lesson learnt here.

robin