I'm running into an issue where the output switching voltage of the LM5155 in the boost configuration will not rise beyond 10% DC regardless of load. That said, without a load, the output rises to my desired voltage, and then shuts off as expected.
Currently I am trying to run it with a Vin = 4V, and a Vout = 14.5V. The inductor is 1uH, and the switching frequency is very close to 1.2MHz. I plan to load it with a 2A load.
These are the scope shots of the loaded converter, where CH1 is the SW pin, and CH2 is the output voltage:
Thoughts?
-Ian Fillinger