Ulrich: This is worth reporting here.
So we had REF come up to 5V. It did not happen with .1uF . We put an extreme value: 1uF
Then we see VREF to 5V
RUN still looked low.
So in order to get fixed probes, I though of soldering short stub at the VREF interconnect.
Power down VBULK.
Get the stub & solder: bam, we see a small arc right at the point where the iron touched the stub!
After that the chip was dead.
Painful proof of our soldering iron being grounded.
Lesson: with high impedance circuits all around, we got to wait before running with a soldering iron in hand on this assembly.
In process of changing the controller - again.
robin
PS: Most likely 2 shorts we reported before must have come about in a similar manner. Bringing in soldering iron too quickly to a pad we suspected did not have good solder wetting...