Hi
We are using BQ25713 in our design, I have some questions on VAP mode. Please help to check,
1. As we all know, VAP mode is enabled in Battery only mode. In my system, I use 2s battery, does VAP mode is valid regardless of Battery status, for example, battery is full or battery is out of power and so on.
2. In DS, It syas " In VAP mode operation, the buck-boost charger delivers the energy from the battery to charge the voltage of the input decoupling capacitors (VBUS) as high as possible (like 20V). " , how could I define OTG output volatge when i using VAP mode ? My 2s battery volatge range is from 7V to 8.4V. I set VBUS voltage to 20V ? Or just 8.4V? How could I set the OTG voltage when battery is full or out of power? Does the VBUS/OTG output voltage could impact the VAP performance?
Thanks.