Other Parts Discussed in Thread: TPS2H160EVM
Dear expert,
Our product containing several TPS2H160A-Q1 as power outputs fails to pass the conducted susceptibility test in the range between 250 KHz and 1.1 MHz.
To investigate the problem, I used the TPS2H160EVM board to reproduce the problem by injecting a 1 Mhz signal generator to the TPS2H160 output.
By injecting a sinus signal on the output, the TPS2H160 does not switch on and generate a fault, this seems act as a current overload. The problem occurs with frequency up to about 3 MHz.
Increasing the current (CL to GND) does little to improve the susceptibility. The power supply is good with decoupling capacitor.
A capacitor (5 - 10 nF) on the output improves a lot.
Do you have a workaround for this problem?
I insert a file with oscillo screen captures
TPS2H160EVM conducted susceptibility problem.docx
Regards
Jean-François