This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92610-Q1: Revisiting previous question concerning SSH and SSL in a circuit to minimize current draw

Part Number: TPS92610-Q1
Other Parts Discussed in Thread: TPS92613-Q1,

In a previous thread, my question was, "I understand that the SSL and SSH are tied together to Out. My question, "If I do not use the Single LED Short Detection feature, what would be the best way to connect SSH and SSL in a circuit to minimize current draw? I need to have current draw low as possible" Wasn't answered completely. It was not mentioned what the maximum resistor divider value could be to minimize current draw."

The response was, "There is no maximum value for the resistor divider. TI recommends total resistance of R1and R2 greater than100-kΩ, so the current has negligible effecton LED luminance. You can use the resistor as large as possible."

My response was, "Interestingly, so even an extreme value of 1 Meg ohm would allow the SSH and SSL inputs to work properly."

There was no response, so I presume it is okay to use  a value of 1 Meg ohm but what about the internal impedance of the TPS92610's SSL and SSH pins? Isn't there a limiting factor? Again, I need to minimize current draw as much as possible and I do not need any of the diagnostic functions.

Thanks