Ulrich:
I looked into the RUN level change with input voltage( DC here), AUX output as well with it.
Up to approx 60V or so, eval kit & ours behave the same.
However, we have to note that the eval kit has a xmfr of low turn ratio. Np:Na is approx 1:0.14 while ours is 1: 0.10
Eval kit Np=21, NA=3t, Ns= 3T, Vbrin around 85V
ours is Np=28, NA=3 T, Ns=1T...Vbrin really should be 350 VDC or so?..Although the calculation I sent used 160 or so...
This means RUN and PWML will come up at a higher input voltage, wouldn't you think so?
But RUN output is not shown to depend upon anything ...since it precedes PWML, the controller has to compare levels at some inputs such as RTZ, BUR etc, right?
I think the xmfr ratios have something to do with RUM & PWML, If the AUX output is not high enough ( i.e. 12V or higher), VDD will not go high enough at all if I keep input VBULK at levels similar to eval kit inputs.
Appreciate any clarification on this.
robin