This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700-Q1: LM74700-Q1

Part Number: LM74700-Q1

Hi

I am planning to use two LM74700-Q1 in ORing application.  Input to one device is 6V battery ( 4x1.5V).  Input to the other device is boost converter output of 6V.   This combination allows one of the sources to be used to drive a brushed motor. 

Do I need the TVS diodes to protect the inputs bearing in mind the battery voltage and boost converter outputs are stable?   Also in the EVM schematic, there are capacitors C2, C3, C4 and D2 .  Would I need them in my application?

Thanks.

Siva