This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: Could you help review UCC2897A schematic?

Part Number: UCC2897A

Hi,

We want to use UCC2897A to design isolated SSR flyback dc-dc ,could you help review our schematic and give your recommendations?  

The attachments are the schematic file and power transformer datasheet.D_762S157001_V02-1.pdfUCC2897ARGPR_ Schematic_20201012.pdf

Requirement as below,

Vin dc=54V

Vout=4V

Iout=7.5A

Note:We referred to our another project and which used PoE TPS2373-4RGWR with UCC2897ARGPR ,we only did some modifications(R122,R128,U102,T101).

Thanks.