This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: UCC28070 no load Consumption

Part Number: UCC28070
Other Parts Discussed in Thread: UCC28064A

HI team

we are realising 900W interleaving PFC  and found that the input W is too large (input 4W)  under 90Vac no-load or 0.0001A

I found that 300W EVM board also has this problem.

Is there a solution?

TKSUCC28070 no load onsumption.docx