This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24296: BQ24196

Part Number: BQ24296


During charging, the led (connected to the STAT pin) started flashing at 1Hz which shows a charging problem.
After disconnecting and reconnecting the charger, the led flashes faster.

Can this be related (as I read in a forum) to the fact that the battery is disconnected and the charger tries to charge the battery and then realizes that it is absent and tries again. Hence a fast flashing on the STAT pin?Thank you