Tool/software: WEBENCH® Design Tools
Hi,
I used the WEBENCH tool to generate the appropriate values for my design(LM5022 Flyback), with the exception of the TR1 transformer, expecting compensation problems, but it turned out that the design didn't work at all. At a power supply of 20 volts, the output transistor T1 is driven by IC1 with narrow pulses (80ns / 8V) with a frequency of about 100kHz and heats up strongly. The output voltages are around zero (0.5 and 0.84 volts) without output load. What could be the reason for this? The data of the transformer are plotted in the diagram.
Regards,
Tsvetan