This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25184-Q1: peak input current ,Power dissipation and temperature rise

Part Number: LM25184-Q1
Other Parts Discussed in Thread: LM25184, LM5155, LM5156

Hello,

We would like to use LM25184-Q1 in our fly back design. 

specification :

Input voltage: Min :12V , Normal :15v ,max :17V

Output voltage :15V 1A   and 7V .25A

Inductance: 20uH, turns ratio

We have used "LM25183 and LM25184 Quickstart Design Tool (Rev. A)" to design the circuit.

Qn 1.For the above specification what would be the peak input current? As per the data sheet the equation for peak current calculation is given below.

As per this calculation the input current comes above 4.1A.Is it possible with LM25184 IC? because the internal mosfet is rated for 4.1A only.

Qn 2:What is the maximum power dissipation capability of the IC LM25184?

Qn 3: what would the temperature rise and thermal dissipation capability of the IC.

Kindly let us know whether we can proceed with the above specification.

Thank you