Other Parts Discussed in Thread: LMG1210
Hi,
we are having a critical issue with LMG1205 during high output current situations.
Basically, we have measured that the HO pin of LMG1205 turns on "high" for apparently no reason, after ~300 ns of HO turning off and keeps latched up high for ~300 ns. This happens only after our system exceeds 50 A, during "short-circuit" situations with 1 µH to GND.
The behavior is "self-sustaining" at a varying frequency between 1 MHz 2 MHz. Obviously, the GaN FETs are destroyed after some milliseconds of this high energy phenomena.
The images explain it.
We have discarded by accurate measurement the following hypothesis:
- Noise on PWM lines: We have added an RC filter and a Schmitt trigger to reject noise glitches. The RC filter is using high-quality 0201 components physically close to LMG1205 and no matter the values the issue persists. Signals confirm that it is not the reason.
- Manufacturing problem: The issue happens with all the samples in 2 manufacturing batches with X-ray testing.
- Gate drive layout: The layout has been done with a lot of love and care following your recommendations but we can make errors...
- The problem is coupling on the GaN FET itself by miller charge?. No: the gate signal is clearly an activation of the device, otherwise the signal would not be a clear 5 V signal. Also it would not explain why the HO keeps active for 300 ns.
Running out of ideas we believe that the only explanation is a kind of malfunction of the LEVEL SHIFT inside LMG1205 circuit due to a too fast or too negative turn-off transient. It looks as the dV/dt or the big negative voltage peak We are aware that these transients exceed the nominal values of LMG1205 but we thought it was ok e2e.ti.com/.../871331
So the solution we are thinking about is:
1. Further reducing layout inductances.
2, Avoid current flowing under the same area as the gate drive.
3. Changing the 0Ω turn-off resistor of the high side to a higher value like 2.2Ω to reduce the speed of the transient.
Really looking forward to your feedback on this issue! Any suggestion or test we can do will be greatly appreciated.
Ernest