This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Team,
Now my customer is using TLV71333 and they are searching LDO part with the latch protection at overcurrent(Vo shorted to GND).
The spec requested of IC is;
VIN range=2.4v - 6V, Programmable VO= 2.4 ~ 3.3V , Iomax=50mA
Is there any recommendation?
Regards,
H.Someno
Hi Someno-san,
Please confirm, but based off of the requirements it seems you are looking for a device that has reverse current protection in the case of a latch-up event. If so then TPS706 would be an excellent choice here.
regards,
Wilson