This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

converter support 19V->0.6Vout with 4A current limit

Other Parts Discussed in Thread: TPS54202, TPS54302

Hello expert,

Do we have solution converter support 19V->0.6Vout with 4A current limit? Thanks!

Best regards,

Ann Lien

  • Hi,

    Here are some recommend can support 19Vin-0.6Vo.

    TPS54202(H): 28V 2A with typ 3.2A HS current limit and typ 3A LS current limit.

    TPS54302/8: 28V 3A with typ 5A HS current limit and typ 4A LS current limit.

    BRs,

    Young