This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260: no12V output

Part Number: TPS54260

Hi team,

below is customer scheamtic, 

without load, the output of TPS54260 can work, and have 12V output

add 120ohm load, the current is about 100mA, output will be drop to 7V from 12V. add heavy load(<1A), the output voltage will drop more.

checked with input 24V is stable, EN pin is high, No PH waveform(always 7V), inductor Isa=3A.

increase boot capacitor to 1uF or 4.7uF, add more output capacitor ,don't any help.

could you help check it and give suggestions? thanks