Other Parts Discussed in Thread: LM74800-Q1, LM74700-Q1
Hi Kari,
In the data sheet of LM 74700, "The breakdown voltage of the TVS+ should be higher than 48-V jump start voltage, less than the absolute maximum ratings of anode and enable pin of LM74700-Q1 (65V) and should withstand 65-V suppressed load dump." That is why SMBJ58A was chosen. If I have a voltage regulator (or a gate driver) after LM74700, and the voltage regulator or the gate driver has a maximum voltage rating of 50-V, instead of the 65-V rating from LM74700, should I adjust TVS+ to SMBJ45A or keep the SMBJ58A? I hope to protect both LM74700 and the voltage regulator or gate driver from the transient voltage damage. Note SMBJ45A has a breakdown voltage of 50-V.
Thanks and I look forward to hearing from you,
John