Other Parts Discussed in Thread: MSP430I2041, TIDM-SERVER-PWR-MON
Hi,
I already asked similar question last year but the requirement was got dropped. We have same requirement so below is the query.
We have to make DC energy meter that is having voltage and current measurement range up to 270V DC and 80A DC respectively.
Accuracy of the DC meter should be 1% across the voltage, current range and operating temperature range of -40C to 70C.
Query:
1. Please suggest metering chip that supports the DC parameter measurement with the specs mentioned above.
2. If there is no metering chip than could you please suggest the solution wherein we can measure the voltage, current , energy parameter.