Other Parts Discussed in Thread: LM74800-Q1
I am using LM76202QPWPRQ1 as a under voltage, over voltage, forward current limiter, and ideal diode to protect power supplies in an automotive application. The device worked as expected until an unsuppressed load dump transient (SAE J1113-11 / ISO 7637-2 pulse 5a) was applied under lab conditions. An oscilloscope probe at the IN pins of the device indicated that peak voltage reached 62 V during the pulse, the maximum input ratings. The LM76202-Q1 device emitted a spark during the pulse and ceased functioning.
There is a 43 V working voltage 6.6kW TVS diode in a DO-218AB package on the power line to LM76202-Q1 input. It is capable of absorbing a large portion of the load dump transient energy, but it appears to not be able to suppress voltage low enough for LM76202-Q1 to survive such a transient.
Please provide suggestions for improved voltage suppression for LM76202-Q1 to survive load dump transients or information on alternate components that have better transient voltage immunity.