This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: TPS82130 reflow/assembly considerations

Part Number: TPS82130

Hello,
I have a couple of questions regarding the 1.53mm height TPS82130 MicroSiP package (μSiL-8 SIL0008D):
- Are there any special reflow/assembly considerations for the μSiL-8 SIL0008D MicroSiP package? Any documents to point to aside from snva853 and slib006?
- MSL level 2 indicates that pre-reflow/assembly baking is not really required with a floor of life less than 1 year @ < 30degC 60%RH?
- what package body thickness applies for the J-STD-033 tables? Total height or laminate substrate thickness only (which is ?)?
- what is the TPS82130 laminate substrate material? Is it FR4?

Kind regards,