Hello,
From the datasheet it seems that the input current can be limited to a maximum of 6.4A. We are using a peak charging current of 8A and system peak current draw is upto 6A. In our case the adaptor current will be feasible only if the adaptor voltage is very high at 24V. using something like a 12V adaptor the input current limit will reduce the charging current significantly. is there a way to disable the input current limit or increase it ?
thank you