This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78PL116: Impact temperature sensor on SOC & RAH calculation

Part Number: BQ78PL116

Hi,

Is the SOC and RAH7FAH are calculated based on temperature? if yes please help me on below queries

1. What happens If the cell Temperature sensors are not connected to BQ78PL116, Does it create any issue in calculation of the SOC and RAH over a period of time?

2. What if the temparature sensor which connected to BQ78PL116 reads more temperature (it used on board temperature sensor(board temperature expected 10-15 more than battery temp))? Does it going to create any problem in the SOC and RAH estimation over a period of time.

Thanks & Regards,

Uday Kumar