This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62864: Package outline

Part Number: TPS62864

Hi Team,

Package outline is shown on both P30 and P37 of the datasheet.
but which should I refer to?
www.ti.com/.../tps62864.pdf


In P30, package dimension is
D: max = 1.8 mm, min = 1.76 mm
E: max = 1.07 mm, min = 1.03 mm

And P37,
D: max = 1.77 mm, min = 1.71 mm
E: max = 1.04 mm, min = 0.98 mm

The form information is different from each other, and I want to confirm which one should refer to.

Beat Regards,
Tom Liu