Part Number: TPS65084
Hi Sir,
The customer want to know if the schematic is correct and any modify or suggestion, thanks for your great support.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65084
Hi Sir,
The customer want to know if the schematic is correct and any modify or suggestion, thanks for your great support.
Hi Tommy,
Thank you for posting. I did quick review based on the schematic checklist, which I recommend customer also to use for layout: https://www.ti.com/lit/zip/slva733
I would recommend:
Overall the schematic closely resembles the Intel reference design which is good. If a layout review is desired, I will require that the layout checklist be filled out and completed with any questions included.
Hi Kevin,
thanks for your great help and reply, if there are any problem, we will learn from you again,thanks.
Hello,
A TPS650842 should work on a TPS650941EVM-116 with the following changes:
Uninstall R36 & Install R37 (BUCKX_1P8V is different for TPS650941 vs. TPS650842)
Uninstall R49 (SWB1 and SWB2 are separate in TPS650842)
Uninstall R67, Install R68 (GPO4 pull-up, probably doesn't matter)
There are a few other changes but I don't expect they would affect functionality:
R26, R35 - ILIM1 & ILIM2 will be wrong, but higher so that should be fine.
BUCK2 output capacitance is higher than needed but that should be fine.
BUCK2 inductor is a 220 nH instead of 330 nH but that should not have a major impact.