Other Parts Discussed in Thread: LM5085, LM5176
I need a DC/DC converter for battery charge.
In detail, CC/CV Mode is needed and the operating parameter is Vin : 53.3 ~ 55 Vdc / Vout : 52.65 Vdc / Idc : 2 A
before, i tried to use lm5085. But i was fail i think because of maximum duty ratio limitation of the ic.
Now, i try to use the lm5176. before make a own design board, i want to confirm the required performance by using lm5176EVM.
Operating range of the EVM module is Vin : 6 ~ 36 Vdc / Vout : 12 Vdc / Idc : 12A / Fsw : 250 kHz.
So, I will change some component for my required performance of DC/DC.
I insult the file about change point. plz check and give any advice.
And also i hope to get simulation file based on TINA under the my parameters.
When i export the simulation file based on TINA from WEBENCH POWER DESIGNER, the results is not as expected.
Looking forward to your reply.lm5176_EVM_Calculator Results.pdflm5176_EVM_Change Components.pdf