I have a custom board based on the UCC28780 reference design. I don't think the upper FET (Q2) is closing. The power supply regulates well under light load up through about 1.2 A. It's supposed to handle up to 2 A out, but it fails if I draw around 1.3 or 1.4 A. I think that's when it transitions from ABM to AAM. I'm attaching my schematic, as well as fab and assembly drawing. I'm also attaching the spreadsheet I used to compute the values. The schematic is "Rev 2" and should match any rework I've done on the Rev 1 board. I can provide raw Altium files, gerbers, etc, if required.
There are two scope captures included in the zip. They were taken with the power supply under a load of 0.6 A. CH1 is the net PWR_VSW; CH2 is either QH_VCC or QH_VDD; CH3 is PWR_PWMH; CH4 is PWR_PWML; MATH is CH2-CH1. The VCC trace (power into the NV6117) looks reasonable. On the other hand, the VDD trace looks terrible. It should be a steady 6.2 V, but it seems to collapse immediately. Have you seen this type of behavior before? Any pointers of where to investigate further, or experiments to run, is appreciated. Thanks!