Hi Team,
Can BQ25703A be used on application scenarios below:
1. Charging: the type-C charger is 5V (the input voltage range is within 5-12V), and the battery is 8.4V in series, which needs boost and fast charging function.
2. When it is not charging, the TYPE-C interface is used as USB host, which power supply to the outside of 5V/1-2A.
Beat Regards,
Tom Liu