This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ripple current selection of the inductor in the buck converter

Other Parts Discussed in Thread: TPS62130A, TPS62180, TPS62184, TPS566238, TPS566231, TPS54620

When designing a buck converter, many application notes recommend that we are supposed to choose a suitable inductance to make the inductor ripple current as 20% to 40% of the Iout. Just want to make sure what the number comes from, is it derived by some mathematic calculations? What will happen if the inductance is larger or smaller? Thanks.

  • Hi Xiaoying,

    I wrote this technical article a while ago, which should answer your question: 

    Power-supply designers have used various forms of Equation 1 for decades in order to select the correct inductance for their step-down (buck) converters. While Equation 1 is still correct, why should you…
    By in Archives > Fully Charged

    Let's look at a specific example.  What Vin, Vout, and Iout do you need a power supply for?

  • Hi Chris,

    Thanks a lot for your great reply!

    I think you have given a great perspective on low-power step-down converters.

    Firstly I am looking at the traditional application, for example, 12V Vin, 3.3V Vout, 2-6A Iout, and the 20% to 40% ripple guarantees CCM condition and reasonable peak current limit.

    Actually I haven't thought about the low-power step-down converters before,  when I look at the datasheet of TPS6213A, I find that there is Table 5 to recommend the inductance. And you say that it requires selecting the inductance to match the compensation for stability. Can you help explain how we choose the inductor considering the stability? Thanks.

    Regards,

    Xiaoying

  • Hi Xiaoying,

    Yes, you are right, stability is also a crucial criteria especially for internally compensated architectures like DCS and DCAP. TPS62130A uses DCS control architecture and needs a certain range of output inductor and output capacitor values to ensure stability.

    Is 6A the maximum current you are looking at? If so, the TPS62130A may not be an option as it can support upto 3A. However, there are many other options which you can check here: https://www.ti.com/power-management/non-isolated-dc-dc-switching-regulators/step-down-buck/buck-converter-integrated-switch/products.html#p238min=1.5;12&p238max=12;30&p451max=6;6&sort=p451max;desc    

    There are newer low cost devices like TPS566231/TPS566238. TPS566238 can allow you to stay in CCM for the entire range of operation by allowing negative inductor currents (check datasheet and Forced PWM operation). For fixed frequency peak current mode control, you can check TPS54620/22 which has external clock synchronization. There are other options like TPS62180/TPS62184 which are dual-phase devices that could be used for greater output voltage accuracy and higher efficiency but need an additional inductor. 

    I would recommend checking out the link above and also try to find out if there are any additional feature requirements for your design. Let us know if you have any more questions.

    Thanks,

    Amod