Hello,
I have a WPT system designed to charge a small battery. the schematic for the system is attached. I found success with this system in a prior revision. I had to redo the entire layout to accommodate a different enclosure though. Now I am finding that I will get my charge and WPT LED to illuminate for a 1 to several seconds, then they start turning off and on at ~1Hz rate. I am also hearing when this occurs a high frequency whine coming from the circuit.
I thought perhaps I'd seen a loss in efficiency from the system due to the layout so I increased Rfod to 300 ohm, I left the Rilim as is for now as I can reduce the charging current allowed allowed from the IC without affecting function of my circuit since I further restrict it with the charge IC.
After doing this I am able to get the device to couple and charge sometimes, not with consistency. When I get successful coupling I do not hear the whine coming from the system. Do you have any suggestions for what may be causing this behavior?
Thanks,
Adam