Other Parts Discussed in Thread: BQ34Z100, , BQ34110, BQ34Z100-G1
Hi TI supporters,
We have a long testing process with BQ34Z100, but in the end we found it might not suitable for our battery design due to the thermistor connection. We are looking for a battery gauge that is able to detect SOC, SOH, FCC, RC etc. We don't want to make any modifications on the batteries for now, so ideally, we hope these parameters are not generated based on the temperature input of the battery cells. But I cannot find any of them, the best suitable one I found is BQ2060A, which has same thermistor wiring as our battery. I cannot find more details on the limiting conditions for this gauge, like the battery charge capacity, number of cells, etc. I couldn't find this gauge when I searched with TI fuel gauges search tool.
The battery we have is NICD, 20 cells in series, nominal cell voltage 1.2V. And the pack has totally of 7Ah and 168 WH.
Please advise any better options or if BQ2060A will meet our requirements.
Thanks,
Charles