Hello, my customer would like to know the external current limit accuracy spec when I(limit) >= 50mA, but when Vvs is operating between 8V to 18V. The datasheet spec is +/-25% (max/min) but this is specified at Vvs = 13.5V. Does current limit accuracy get worse than this when Vvs is between 8V to 18V, and is there test data that shows the variation across Vvs range?
Also, if they use a CL resistor of 2.55kohm to set a nominal current limit of 94mA and the load current slowly increases, should they expect the current to overshoot by up 1.5x higher than the setpoint (or ~140mA)?
Thanks,
Alan