Hi Team,
Our customer first inquiry is if the BQ75570 VIN_DC input be connected to a power supply (5V) instead of solar panel. They like to bench test our devices indoors to ensure they're working yet keep their battery topped off, so replacing the solar panel with a 5V power source would enable us to do this.
We answer the customer using this thread below:
https://e2e.ti.com/support/power-management/f/196/t/787040
After sharing the thread above, the customer would like to confirm if connecting any typical 4.2V LiPo charger ~250mA and that will do the trick?
Another question is what are the consequences of connecting a 6V panel to the BQ25570?
They don't have anything connected to VOUT so not using the buck converter and have 4.2V LiPo connected to VBAT with its own over-voltage protection circuitry.
Here's the customer schematic for your reference:
EclipseSolarEV3.pdf
Please let me know if you have any questions with the customer.
Thanks,
Jonathan
what are the consequences of connecting a 6V panel to the BQ25570?