Other Parts Discussed in Thread: AM3358, , TPS65218D0, BQ25910, BQ25792, BQ25616
Hi,
we have a custom board with AM3358 and TPS65217D PMIC. On our board we will integrate Lipol battery at 8000mAh capacity. We noticed that charger functionality of PMIC is kind of limited.
We need following functionality:
1. Monitor fuel gauge of our battery -> we will use BQ27220 as it was proposed in other question https://e2e.ti.com/support/power-management/f/196/t/970510
2. Charge battery via USB, charge it even when board is shutdown. (Keeping pb_in button for 8 secodns) -> From the TRM of PMIC we understood when pb_in is held for 8 seconds, the chip goes to off state and charging is turned off.
3. Control LED with charging status. Charging ON -> LED on, charging off or battery full -> LED off. This is not easily achievable with PMIC as there is no status pin. The LED must be controlled via HW as the board can be turned off.
We looked for external charger IC. It seems that it would solve our issues and provides even higher charging current e.g. 3A as a USB standard.
Am I correct that for our purpose PMIC charger is not suitable and we should really go with some external charger IC?
What charger would you recommend us to use, if we have single cell lipol battery?
Is there an option to use one IC with charger and fuel gauge integrated inside?
Should the power management path be solved in external charger IC or still in PMIC?
Thanks for any hints.