This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: Vsys could not be limited to SYSmin When remove the battery and use 5V adatpter as only power source

Part Number: BQ25713

Hi Team,

i met a problem while debuging the BQ25713:

The main problem is blow:

we remove the 2s battery and only use 5v adapter as power source.

we found that the Vsys would drop with the system current rise and we also could not limite the Vsys above the SYSmin. i attached the Log under two working condition.

Situation1: Vin=5V  with no load

reg[ 0]=0xa

 

reg[0x1]=0x87

 

reg[0x2]=0xc0

 

reg[0x3]=0x7

 

reg[0x4]=0xd0

 

reg[0x5]=0x20

 

reg[0x6]= 0

 

reg[0x7]= 0

 

reg[0x8]= 0

 

reg[0x9]= 0

 

reg[0xa]= 0

 

reg[0xb]=0x2

 

reg[0xc]= 0

 

reg[0xd]=0x18

 

reg[0xe]= 0

 

reg[0xf]=0x41

 

reg[0x10]=0xff

 

reg[0x11]=0xff

 

reg[0x12]=0xff

 

reg[0x13]=0xff

 

reg[0x14]=0xff

 

reg[0x15]=0xff

 

reg[0x16]=0xff

 

reg[0x17]=0xff

 

reg[0x18]=0xff

 

reg[0x19]=0xff

 

reg[0x1a]=0xff

 

reg[0x1b]=0xff

 

reg[0x1c]=0xff

 

reg[0x1d]=0xff

 

reg[0x1e]=0xff

 

reg[0x1f]=0xff

 

reg[0x20]= 0

 

reg[0x21]=0x84

 

reg[0x22]= 0

 

reg[0x23]=0xa8

 

reg[0x24]= 0

 

reg[0x25]=0x41

 

reg[0x26]= 0

 

reg[0x27]=0x1f

 

reg[0x28]= 0

 

reg[0x29]= 0

 

reg[0x2a]= 0

 

reg[0x2b]= 0

 

reg[0x2c]=0x57

 

reg[0x2d]=0x57

 

reg[0x2e]=0x40

 

reg[0x2f]=0x88

 

reg[0x30]=0x10

 

reg[0x31]=0x2

 

reg[0x32]=0xb7

 

reg[0x33]=0x2

 

reg[0x34]=0x30

 

reg[0x35]= 0

 

reg[0x36]=0x65

 

reg[0x37]=0x4a

 

reg[0x38]=0xa0

 

reg[0x39]=0x81

 

reg[0x3a]=0xff

Situaiton2: Vin=5v with system load:  

[2021-02-20_17:28:32]reg[ 0]=0xa

 

[2021-02-20_17:28:32]reg[0x1]=0x87

 

[2021-02-20_17:28:32]reg[0x2]=0xc0

 

[2021-02-20_17:28:32]reg[0x3]=0x7

 

[2021-02-20_17:28:32]reg[0x4]=0xd0

 

[2021-02-20_17:28:32]reg[0x5]=0x20

 

[2021-02-20_17:28:32]reg[0x6]= 0

 

[2021-02-20_17:28:32]reg[0x7]= 0

 

[2021-02-20_17:28:32]reg[0x8]= 0

 

[2021-02-20_17:28:32]reg[0x9]= 0

 

[2021-02-20_17:28:32]reg[0xa]= 0

 

[2021-02-20_17:28:32]reg[0xb]=0x2

 

[2021-02-20_17:28:32]reg[0xc]= 0

 

[2021-02-20_17:28:32]reg[0xd]=0x18

 

[2021-02-20_17:28:32]reg[0xe]= 0

 

[2021-02-20_17:28:32]reg[0xf]=0x41

 

[2021-02-20_17:28:32]reg[0x10]=0xff

 

[2021-02-20_17:28:32]reg[0x11]=0xff

 

[2021-02-20_17:28:32]reg[0x12]=0xff

 

[2021-02-20_17:28:32]reg[0x13]=0xff

 

[2021-02-20_17:28:32]reg[0x14]=0xff

 

[2021-02-20_17:28:32]reg[0x15]=0xff

 

[2021-02-20_17:28:32]reg[0x16]=0xff

 

[2021-02-20_17:28:32]reg[0x17]=0xff

 

[2021-02-20_17:28:32]reg[0x18]=0xff

 

[2021-02-20_17:28:32]reg[0x19]=0xff

 

[2021-02-20_17:28:32]reg[0x1a]=0xff

 

[2021-02-20_17:28:32]reg[0x1b]=0xff

 

[2021-02-20_17:28:32]reg[0x1c]=0xff

 

[2021-02-20_17:28:32]reg[0x1d]=0xff

 

[2021-02-20_17:28:32]reg[0x1e]=0xff

 

[2021-02-20_17:28:32]reg[0x1f]=0xff

 

[2021-02-20_17:28:32]reg[0x20]= 0

 

[2021-02-20_17:28:32]reg[0x21]=0x8c

 

[2021-02-20_17:28:32]reg[0x22]= 0

 

[2021-02-20_17:28:32]reg[0x23]=0xa8

 

[2021-02-20_17:28:32]reg[0x24]= 0

 

[2021-02-20_17:28:32]reg[0x25]=0x41

 

[2021-02-20_17:28:32]reg[0x26]= 0

 

[2021-02-20_17:28:32]reg[0x27]=0x1c

 

[2021-02-20_17:28:32]reg[0x28]= 0

 

[2021-02-20_17:28:32]reg[0x29]= 0

 

[2021-02-20_17:28:32]reg[0x2a]= 0

 

[2021-02-20_17:28:32]reg[0x2b]=0x6

 

[2021-02-20_17:28:32]reg[0x2c]=0x5

 

[2021-02-20_17:28:32]reg[0x2d]=0x9

 

[2021-02-20_17:28:32]reg[0x2e]=0x40

 

[2021-02-20_17:28:32]reg[0x2f]=0x88

 

[2021-02-20_17:28:32]reg[0x30]=0x10

 

[2021-02-20_17:28:32]reg[0x31]=0x2

 

[2021-02-20_17:28:32]reg[0x32]=0xb7

 

[2021-02-20_17:28:32]reg[0x33]=0x2

 

[2021-02-20_17:28:32]reg[0x34]=0x30

 

[2021-02-20_17:28:32]reg[0x35]= 0

 

[2021-02-20_17:28:32]reg[0x36]=0x65

 

[2021-02-20_17:28:32]reg[0x37]=0x4a

also i attached the schematic below:

5025.charger.pdf

i may need you help on finding the rount cause and therefore find a way to solve.

BR

Brandon