Hi team,
If my customer calculates the max junction temperature for their application with a constant current, they are above the maximum temperature. They would like to know how this can be calculated in function of the “driving” time?
Their specs are as follws:
Imax: 5A (no high side limitation)
Tmax: 50 or 100ms
Rdson_max: 166mOhm
Ta max: 85°C
Roja: 35 °C/W @100mm2 4layers
Tshutdown: 175°C
Worst case junction temperature
Do you have any suggestion?
Thanks for the help.
Obinna.