Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: Charging and using 8 18650 cell in parallel

Part Number: BQ25895

Hi,

We need to use 8 18650 cells in parallel in one of our project. This 8 cells will be replaceable and will be connected to each other in parallel creating a 3.7V 20.8Ah battery capacity.

Below are my queries related to the use case:

1) Can we use a single cell charger IC (e.g: bq25895) for 8 cells in parallel?

2) DO we have to use a BMS for parallel cell options?

3) Our use case is similar to the power bank. But, the User will have an option to replace the cells if needed. Could you let us know if we need to take care of any extra protection?

4) We are going to design a customer PCM circuit for the OCD, OVP and other needed protection for all 8 cells together. Let us know if we need to add anything else too.

Regards,

Mayur