I am working a boost converter with 2.7V-3.6V input range, with a nominal 12V dc output with nominal load < 50mA / step-load fo 500mA for < 100mS.
The boost converter works okay and reaches 12V output with a low load at Vin > 3.2Vdc, but when Vin < 3.2Vdc, it drops down to 10V, and at 2.7Vdc in, it drops to 6Vdc but it is still switching at 600kHz.
The inductor value is 10uH with Isat / Irms 5.5A.
On the scope, the current drawn by the boost increases as the voltage goes up from 3V to 3.6Vdc to around 1.5A and drops to 200mA when at 2.7Vdc.
Is the IC capable of operating in this condition and providing a 12Vdc output even in PFM mode with < 10mA load current? The datasheet shows that the IC will go up to target Vout x 1.125 voltage then switch to PFM mode.
Some technical guidance is required urgently please.